Digital Video

Time Slicing Structure

Time Slicing Structure is defined in Annex M in ETSI EN 302 307-1. It is a technique within the DVB-S2 standard that allows receivers to select specific streams within a wideband signal at the physical layer, rather than needing to process the entire signal. The transmitter shall map the input services into streams (identified by a specific Time Slice Number, TSN). Such streams shall be transmitted in time slices (i.e. bursts) suitably spaced in time. A time-slicing burst (identified by a specific TSN) shall correspond to one PL-Frame. Time-slicing mode shall comply with the conventional DVB-S2/S2X, with the exception of the PL Signaling.

The PLHEADER shall be extended to two SLOTs of 90 symbols (180 symbols), composed of the following fields:

        => puncture from 80 bits to 77 bits as follows:

1 0 1 1 1 1 0 0 0 0 0 1 0 0 0 1 1 0 0 0 0 0 0 0 1 0 1 0 0 1 0 1 0 1 0 1 0 0 0 1 0 1 1 1 0 1 1 1 0 1 0 1 1 1 0 0 1 0 0 1 1 1 0 1 1 0 0 0 0 1 0 1 1 0 0 0 1 1 1 1 1 1 0 1 1 0 1 0 1 1 0 0 1 1 0 1 1 0 1 1 1 0 0 0 0 1 1 1 0 0 0 1 1 0 1 0 1 0 0 1 1 1 1 1 0 0 0 1 0 0 0 0 1 1 0 0 1 0 1 0 0 0 0 0 0 1 1 1 1 0 1 1 1 1

, , for

When the Time Slicing Structure is set to ON, you can set the Time Slicing Pattern (with TSL index) to decide the actual permutation of multiple PLFrames with different TSN. Corresponding TSN and MODCOD sequences will also be shown below. The PLFRAME length for each TSL will be calculated. For example, the Time Slicing Sequence is [1, 2, 3, 4, 3, 1] by TSL index. Actual waveform generation and playback pattern by TSN: [0x01, 0x10, 0x20, 0x30, 0x20, 0x01]. If one specific receiver would only receive input stream with TSN 0x01, then it would decode the 1st and 6th PLFrames in the total 6 frames.

Name

Ranges

Note

Time Slicing Structure

Off | On

Default is Off.

TSL Sequence

1 ~ number of TSLs

It can be an array when the number of TSLs is more than one.

TSN(Hex) Sequence

 

Read-only. It can be an array when the number of TSLs is more than one.

MODCOD Sequence

 

Read-only. It can be an array when the number of TSLs is more than one.

PLFRAME Length Sequence

 

Read-only. It can be an array when the number of TSLs is more than one.

In time slicing mode, parameters VL-SNR, MODCOD, FEC, Pilot and Payload under "DVB-S2/S2X Settings" will be hidden, and they should be configured separately for each TSLs. The PLFRAME Length for each TSL will be computed accordingly. New TSL tree-node will be added with Add/Remove/Copy toolbar actions to support multiple TSLs. For Payload Data Source Type, only Test Pattern and Binary Pattern File are supported.

Name

Ranges

Note

TSL

0x00 to 0xFF

Read-only, unique for each TSL configuration

Time Slicing Number (Hex)

0x00 to 0xFF

TSLs with the same TSN should have the same MODCOD values.

Insert VL-SNR Header

Same as in DVB-S2/S2X Settings

FEC Frame

Modulation Type

Code Rate

Insert Pilot

PLFRAME Length

Read-only, calculated by current TSL configuration.

Payload

Only Test Pattern and Binary Pattern File are supported.